LTE TDD

Full-filled Config (Basic TDD)

For Waveform Playback (ARB) capability.

The Full-filled Preset Config configures all resource blocks with QPSK data, filling the available bandwidth. This dialog box is accessible by clicking the Full-filled Config button displayed in the toolbar when the Uplink or Downlink node is selected for a Basic TDD carrier.

Full-Filled Config

Applies the Full-filled QPSK preset, which allocates all available RBs with QPSK modulation to a DL-SCH transport channel. This is a one-shot action command with no query.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:CONFig:FFILled "<string>"

SCPI Example

RADio:LTETdd:WAVeform:CCARrier1:CONFig:FFILled "SystemBandwidth:B5M,Modulation:QPSK"

Notes

Fills both DL (PDSCH) and UL (PUSCH) with the selected modulation across all RBs.

Comma-separated key:value.

Keys: SystemBandwidth (B1M4|B3M|B5M|B10M|B15M|B20M), Modulation (QPSK|QAM16|QAM64|QAM256).

Same command is used for both DL and UL Full-Filled Config buttons.

Preset

N/A

State Saved

No

Initial S/W Revision

A.20.01

Carrier Uplink (Basic TDD)

Carrier Downlink (Basic TDD)

Welcome to LTE TDD